Montreal, Canada – Future Electronics, a global leading distributor of electronic components, is promoting the simple and highly-configurable NCS32100 rotary position sensor through a chance to win an evaluation kit to test and prototype related designs.
An NCS32100 evaluation kit is a hardware and software package designed to allow developers to evaluate the capabilities of the NCS32100 microcontroller and create proof-of-concept designs. The kit typically includes a development board with an NCS32100 microcontroller and various peripherals, such as memory, input/output (I/O) interfaces, and communication interfaces. It may also include software tools, such as a compiler and debugger, and documentation to help users get started with the NCS32100.
The NCS32100 is a microcontroller produced by onsemi. It is a 32-bit, RISC-based processor with on-chip memory, various peripherals, and a range of communication interfaces. The NCS32100 is designed for use in embedded systems and other applications that require a low-power, high-performance processor. It is often used in a wide range of devices, including Internet of Things (IoT) devices, industrial control systems, and consumer electronics.
To learn more about the Evaluation Kit and get a chance to win one, visit content.futureelectronics.com/resources/featured-products/onsemi-evaluation-kit-for-ncs32100-position-sensor.
For more information about Future Electronics and its 170 office locations in 44 countries around the world, visit www.FutureElectronics.com.