Panasonic’s ECQ-UA Series Film Capacitors Featured in Latest Lighting Newsletter

Montreal, Canada – Future Electronics, a global leading distributor of electronic components, is featuring advanced Film Capacitors from Panasonic in this month’s Lighting newsletter.

Panasonic’s ECQ-UA Series Metallized Polypropylene Film Capacitors benefit from an original in-house patterned metallization process with a fuse mechanism function. This unique technology delivers stable capacitance levels over the product lifetime and higher reliability of the application.

These ECQ-UA Series Film Capacitors feature an operating temperature range of -40°C to 110°C, a rated voltage of 275V.AC up to 310 V.AC and a nominal capacitance range of 0.1μF up to 10μF. A flame-retardant plastic case and non-combustible resin are utilized leading to accreditation under UL/CSA and European safety regulation for Class X2. All the products are fully RoHS and REACH compliant.

The ECQ-UA Series is ideal for a broad spectrum of applications including input/output filtering for charging stations or the input side of On-Board chargers, industrial power supplies, the range of EV/PHEV applications, and renewable energy infrastructure. AEC-Q200 compliance ensures that these Film Capacitors meet the most stringent quality standards in the industry.

To learn more, visit, https://content.futureelectronics.com/resources/featured-products/panasonic-ecq-ua-series. To see the entire portfolio of Panasonic products available through Future Electronics, visit www.FutureElectronics.com.

The Lighting newsletter is packed with product information, datasheets and videos showcasing the most advanced innovations. To receive upcoming issues of the Lighting newsletter, and to stay up to date with the latest lighting innovations, visit www.FutureElectronics.com/subscribe.

About Future Electronics

Future Electronics is a global leader in the electronic components industry. The company’s award-winning customer service, comprehensive global supply chain programs, and industry leading engineering design expertise make it a strategic partner of choice for customers worldwide.

A WT Microelectronics company, Future Electronics is headquartered in Montreal, Canada, and operates in 44 countries and 159 offices. Its global footprint enables exceptional service and efficient, end to end supply chain solutions. The company is fully integrated and supported by a single IT infrastructure that provides real-time inventory visibility and seamless global operations, sales, and marketing capabilities.

For more information, visit www.FutureElectronics.com.

Media Contact

Jamie Singerman

Corporate Vice President Worldwide

Future Electronics

www.FutureElectronics.com

514-694-7710

Fax: 514-693-6051

Jamie.Singerman@FutureElectronics.com