Power Integrations BridgeSwitch Family of Integrated Half-Bridges Featured By Future Electronics In THE EDGE

Montreal, Canada – Future Electronics, a leading global distributor of electronic components, releases its industry-leading tech newsletter, THE EDGE, twice a month. The Power Integrations BridgeSwitch family of integrated half-bridges was featured in the most recent edition.

The Power Integrations BridgeSwitch family of integrated half-bridges dramatically enhances the development and production of high-voltage inverter-driven one or three-phase PM or BLDC motor drives.

These half-bridges incorporate two high-voltage N-channel power FREDFETs with low and high-side drivers in a single small-outline package. The internal power FREDFETs offer ultra-soft and ultrafast diodes ideally suited for hard-switched inverter drives. Both drivers are self-supplied eliminating the need for an external auxiliary power supply.

BridgeSwitch provides a unique instantaneous phase current output signal simplifying implementation of sensor-less control schemes. The low-profile, compact footprint surface mount package offers extended creepage distances and allows heat sinking of both power FREDFETs through the printed circuit board. BridgeSwitch also offers internal fault protection functions and external system-level monitoring. The bi-directional bussed single wire status interface reports observed status changes.

Features of the Power Integrations BridgeSwitch include a status interface, enhanced safety and reliability features, and the highest performance and design flexibility. Applications include one or three-phase high-voltage PM and BLDC motor drives, up to 400W typical inverter output power, appliances including dishwashers and refrigerators, condenser fans in air conditioners, and more.

To read more features and tech specs of the Power Integrations BridgeSwitch family of integrated half-bridges please visit https://content.futureelectronics.com/resources/featured-products/power-integrations-bridgeswitch-family-of-integrated-half-bridges. To view the entire portfolio of products available through Future Electronics, visit http://www.FutureElectronics.com.

THE EDGE is the latest e-newsletter from Future Electronics and is geared toward engineers and buyers looking for new or leading-edge products. THE EDGE comes out twice per month, and each edition features product information, datasheets and videos showcasing the most advanced new technology in a specific area, such as sensing, lighting, or automotive. Register here to receive the latest issues of THE EDGE newsletter, and stay up to date with the newest technologies.

About Future Electronics

Future Electronics is a global leader in the electronic components industry. The company’s award-winning customer service, comprehensive global supply chain programs, and industry leading engineering design expertise make it a strategic partner of choice for customers worldwide.

A WT Microelectronics company, Future Electronics is headquartered in Montreal, Canada, and operates in 44 countries and 159 offices. Its global footprint enables exceptional service and efficient, end to end supply chain solutions. The company is fully integrated and supported by a single IT infrastructure that provides real-time inventory visibility and seamless global operations, sales, and marketing capabilities.

For more information, visit www.FutureElectronics.com.

Media Contact

Jamie Singerman

Corporate Vice President Worldwide

Future Electronics

www.FutureElectronics.com

514-694-7710

Fax: 514-693-6051

Jamie.Singerman@FutureElectronics.com