Montreal, Canada – Future Electronics, a global leading distributor of electronic components, is featuring advanced capacitors from Panasonic in the latest edition of THE EDGE – Transportation.
Panasonic’s EZP-V Series Metallized Polypropylene Plastic Film Capacitors feature a built-in fuse function combined with a small case size, which makes them ideal for applications requiring DC linkage. Built-in fuse functionality ensures that EZP-V Series parts open in the event of an unlikely failure, rather than creating a short circuit situation.
EZP-V Series capacitors deliver the stability and reliability needed for major applications such as solar inverters and wind power generation. Key highlights include a wide operating temperature range of -40°C up to +105°C, a rated voltage range of 600VDC to 1100VDC and a nominal capacitance range of 3µF up to 110µF.
To learn more, visit, content.futureelectronics.com/resources/featured-products/panasonic-ezp-v-metallized-polypropylene-plastic-film-capacitors. To see the entire portfolio of Panasonic products available through Future Electronics, visit www.FutureElectronics.com.
THE EDGE is the latest e-newsletter from Future Electronics, and is geared toward engineers and buyers looking for new or leading-edge products. THE EDGE comes out twice per month, and each edition features product information, datasheets and videos showcasing the most advanced new technology in a specific area, such as sensing, lighting, or automotive.
Visit www.FutureElectronics.com/subscribe to receive the latest issues of THE EDGE newsletter, and stay up to date with the newest technologies.