Future Electronics Features Melexis MLX90416 Single-Coil 24 V 60 W Code-Free Fan Driver

Montreal, Canada – Future Electronics, a leading global distributor of electronic components, is pleased to announce the launch of a new digital campaign featuring the Melexis MLX90416 single-coil, code-free fan driver IC. Engineered to simplify motor control design, the MLX90416 delivers reliable performance for 12 V and 24 V fan and pump applications across industrial and consumer markets.

The MLX90416 integrates two low-RDS(on) half-bridges and supports up to 8 A braking current with a programmable current limit of up to 4 A—often eliminating the need for an external TVS. Operating via PWM control, it offers programmable FG output for speed feedback, eight speed curve configuration points, and speeds up to 40 k mRPM for 2 pole-pair motors. Its embedded non-volatile memory, programmable via I²C, enables multiple updates and streamlined development.

Robust protection features include Locked Rotor Protection, Under-Voltage Protection with hot unplug handling, Thermal Shutdown, and Overcurrent Protection. The code-free, plug-and-play architecture eliminates complex MCU-based software validation, reducing development time and accelerating time-to-market.

For easy evaluation and programming, Melexis provides the FandriverEVB2 for device control and the FandriverProgrammerB for mass programming, along with a GUI that includes a built-in motor parameter extraction tool.

This new digital campaign highlights how the Melexis MLX90416 helps engineers design efficient, compact fan and pump solutions with minimal development effort.

For more information about the Melexis MLX90416 single-coil fan driver and to explore the full campaign, visit the dedicated campaign landing page.

About Future Electronics

Future Electronics is a global leader in the electronic components industry. The company’s award-winning customer service, comprehensive global supply chain programs, and industry leading engineering design expertise make it a strategic partner of choice for customers worldwide.

A WT Microelectronics company, Future Electronics is headquartered in Montreal, Canada, and operates in 44 countries and 159 offices. Its global footprint enables exceptional service and efficient, end to end supply chain solutions. The company is fully integrated and supported by a single IT infrastructure that provides real-time inventory visibility and seamless global operations, sales, and marketing capabilities.

For more information, visit www.FutureElectronics.com.

Media Contact

Jamie Singerman

Corporate Vice President Worldwide

Future Electronics

www.FutureElectronics.com

514-694-7710

Fax: 514-693-6051

Jamie.Singerman@FutureElectronics.com