Engineering Insights & Hands-On Demos

TechVentures

Video Series

With Lazina Rahman

Hands-On Demos & Expert Engineering Insights

Embedded World 2022: NXP IW612, the World’s First True Tri-Radio Wireless SoC Device

In this TechVentures video, Future Electronics’ Technical Marketing Engineer Lazina Rahman visited the NXP booth at Embedded World 2022 to explore an industry-first solution by NXP.

Lazina checked in with Max Palumbo, Product Marketing Specialist for NXP Semiconductors, to walk us through the full capabilities of the newly-launched IW612, an industry-first tri-radio SoC to run Wi-Fi 6, BLE 5.2 Audio and 802.15.4 Thread concurrently.

The NXP IW612 brings higher throughput, better network efficiency, lower latency and improved range over previous generation Wi-Fi standards.

The device includes a full-feature Wi-Fi subsystem powered by their 802.11ax (Wi-Fi 6) technology. The SoC integrates a Wi-Fi MAC and also includes baseband as well as direct-conversion radio with integrated PA, LNA and a transmit/receive switch which removes the need for an RF front-end module (FEMs). This significantly reduces costs and system complexity.

Here is the NXP IW612 internal block diagram.

Enjoyed this episode?

Subscribe to the TechVentures with Lazina YouTube series for more hands-on demos and engineering insights.

Enjoyed this episode?

Subscribe to the TechVentures with Lazina YouTube series for more hands-on demos and engineering insights.

More Episodes

Need Engineering Expertise?

Whether you're evaluating technologies, modernizing infrastructure, or accelerating a deployment, our engineering specialists can help turn ideas into real-world solutions.